MC9S08DN16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,132件の閲覧回数
vikassubramani
Contributor II

Hi every body i am a new bie to MC9S08DN16 controller and i am facing problem in toggling the port the code is as below.

 

/* [sample program to toggle the port D of the micro controller ] */

 

#include <hidef.h> /* for EnableInterrupts macro */

#include "derivative.h" /* include peripheral declarations */

void port_initialize(void);

void delay(void);

 

 

void main(void)

{

  EnableInterrupts;

  /* include your code here */

  port_initialize();

  while(1)

  {

  PTED = 0x00; /* flashing 0's on to port D */

  delay();   /* delay function */

  PTED = 0xff; /* flashing 1's on to port D */

  delay(); /* delay function */

  }

   /* loop forever */

  /* please make sure that you never leave main */

}

 

 

void port_initialize(void )

{

  PTEDD = 0xff; /* port D data direction register configured as output */

  PTEPE = 0x00; /* Internal pull-up/pull-down device disabled for port D */

  PTESE = 0x00; /* Output slew rate control disabled for port D */

// PTEPE = 0x00; /* Port disabled as interrupt */

}

 

 

void delay()

{

  unsigned int i,j;

  for(i=0; i<255; i++)

  for(j=0; j<255;j++);

}

 

 

 

The problem i am facing is that although the code is in infinate loop. when i run the program after few seconds the code will exit unexpectedly and will lead to a new window and displays the following.

 

 

#pragma NO_EXIT

__EXTERN_C void _Startup(void) {

/* set the reset vector to _Startup in the linker parameter file (*.prm):

    'VECTOR 0 _Startup'

 

 

    purpose:    1)  initialize the stack

                2)  initialize run-time, ...

                    initialize the RAM, copy down init data, etc (Init)

                3)  call main;

    called from: _PRESTART-code generated by the Linker

*/

  INIT_SP_FROM_STARTUP_DESC(); /*lint !e960 MISRA 14.3 REQ, not a null statement (instead: several HLI statements) */

 

#ifndef  __ONLY_INIT_SP

  Init(); /*lint !e522 function 'Init' contains inline assembly */

#endif

#ifndef __BANKED__

  __asm JMP main;  /* with a C style main(); we would push the return address on the stack wasting 2 RAM bytes */

#else

  __asm CALL main;

#endif

}

ラベル(1)
0 件の賞賛
返信
1 解決策
1,902件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Vikas,

from your description, your program got reset when running in loop.

I wonder the reset was caused by COP. please try to add feed dog code inside for() loop:

for example:;

  for(;;) {

... ...

    __RESET_WATCHDOG(); /* feeds the dog */

... ...

  } /* loop forever */

this can avoid watchdog reset.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,903件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Vikas,

from your description, your program got reset when running in loop.

I wonder the reset was caused by COP. please try to add feed dog code inside for() loop:

for example:;

  for(;;) {

... ...

    __RESET_WATCHDOG(); /* feeds the dog */

... ...

  } /* loop forever */

this can avoid watchdog reset.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

0 件の賞賛
返信
1,902件の閲覧回数
vikassubramani
Contributor II

thanks zhang jennie the problem was solved

0 件の賞賛
返信
1,902件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome.

Best Regards,

Jennie

0 件の賞賛
返信