MC9S08AC60 will not load data from EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08AC60 will not load data from EEPROM

3,199件の閲覧回数
wtyler
Contributor I

I am currently using a MC9S08AC60 to control a Key Pad and display. The problem is after a while the Micro will not load the the 4KB EEPROM graphics data to the display after a KBI1P4/PTG4 is triggered.

0 件の賞賛
返信
4 返答(返信)

3,182件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

can you please give me more information about the problem

are you using an external eeprom? 

are you using SPI or IIC to load the data on the EEPROM?

 

regards

0 件の賞賛
返信

3,134件の閲覧回数
wtyler
Contributor I

Can you please give me more information about the problem: After the micro processes an IRQ there is no MOSI/MISO data activity.

Are you using an external EEPROM: Yes after the Micro IRQ the data from the Micro is loaded to the EEPROM through a level shifter to a graphic display. Problem is the graphic data is not displayed from the Micro.

Are you using SPI or llC to load the data on the EEPROM: I Sam using SPI MOSI/MISO to load the EEPROM

0 件の賞賛
返信

3,121件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Can you check if the data is sending properly on the SPI to the EEPROM?

Do you have any flag pending?

 

have a good day

 

0 件の賞賛
返信

3,110件の閲覧回数
wtyler
Contributor I

After the IRQ no data is sent to the EEPROM. I don’t know how to check the flags.

0 件の賞賛
返信