MC9S08AC60 will not load data from EEPROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08AC60 will not load data from EEPROM

3,186 Views
wtyler
Contributor I

I am currently using a MC9S08AC60 to control a Key Pad and display. The problem is after a while the Micro will not load the the 4KB EEPROM graphics data to the display after a KBI1P4/PTG4 is triggered.

0 Kudos
Reply
4 Replies

3,169 Views
vicentegomez
NXP TechSupport
NXP TechSupport

can you please give me more information about the problem

are you using an external eeprom? 

are you using SPI or IIC to load the data on the EEPROM?

 

regards

0 Kudos
Reply

3,121 Views
wtyler
Contributor I

Can you please give me more information about the problem: After the micro processes an IRQ there is no MOSI/MISO data activity.

Are you using an external EEPROM: Yes after the Micro IRQ the data from the Micro is loaded to the EEPROM through a level shifter to a graphic display. Problem is the graphic data is not displayed from the Micro.

Are you using SPI or llC to load the data on the EEPROM: I Sam using SPI MOSI/MISO to load the EEPROM

0 Kudos
Reply

3,108 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Can you check if the data is sending properly on the SPI to the EEPROM?

Do you have any flag pending?

 

have a good day

 

0 Kudos
Reply

3,097 Views
wtyler
Contributor I

After the IRQ no data is sent to the EEPROM. I don’t know how to check the flags.

0 Kudos
Reply