MC1321x question using it.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC1321x question using it.

2,212 Views
Xirdneh
Contributor I
Im currently trying to make a proyect in robotics. What I want to do with Zegbee is preatty simple, just tu control some servo motors and a couple of control lines regarding proximity sensors. The thing is that im a student and Im trying to keep costs low, so i have ordered the MC13212 sample, it arrives tomorrow. But now, how am I suppouse to programm it?, and do I need a Zigbee Stack?, if I do can i Use the TI Z-Stack, condiering it is free. Other thing, if I need a Serial interface to programm the MCU then where can I get a usb-serial cable that can take care of the comunication between the MCU and my Lap. Thank You.
Labels (1)
0 Kudos
Reply
2 Replies

1,579 Views
addiyi
NXP Employee
NXP Employee
For programming a board that use MC13212 , will need to have CodeWarrior (to write your applications) and a BDM (download your applications into the board). You can try to use SMAC4.2, with contain example applications and is free for download.

Regards,
Adrian
0 Kudos
Reply

1,579 Views
Neo
Contributor I
Dear Adrian:
 
I have trouble compiling Accel_V3.0 and Wireless Uart SMAC 4.2 project in the CodeWarrior (V5.9).
There were too many errors and warnings.
Could you send me the compiled .s19 file?
0 Kudos
Reply