MC13213 power comsuption problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC13213 power comsuption problem

1,737件の閲覧回数
morgana
Contributor I
Hi,
 
I have designed a  custom Zigbee board using the reference designs of freescale for the MC13213 . The Zigbee network is created and the nodes can communicates. The problem is that in the precise point in which the network is created the consumption of current goes from 20-30mA to 50-60mA. I'm using both stacks, the older: Figure8Wireless and the new BeeStack and with both the results is the same: 60mA. I've already check the register status and it seem's ok. I need to know if someone had made a custom board with a normal comsuption: 30-37mA.
 
Greetings
Ing. Morgana
ラベル(1)
0 件の賞賛
返信
1 返信

1,019件の閲覧回数
Alban
Senior Contributor II
Hello,

I am afraid that you are unlikely to receive feedback from your schematics as it is in a quality that does not allow characters to be read.

Cheers,
Alban.
0 件の賞賛
返信