MC13213 power comsuption problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13213 power comsuption problem

1,747 Views
morgana
Contributor I
Hi,
 
I have designed a  custom Zigbee board using the reference designs of freescale for the MC13213 . The Zigbee network is created and the nodes can communicates. The problem is that in the precise point in which the network is created the consumption of current goes from 20-30mA to 50-60mA. I'm using both stacks, the older: Figure8Wireless and the new BeeStack and with both the results is the same: 60mA. I've already check the register status and it seem's ok. I need to know if someone had made a custom board with a normal comsuption: 30-37mA.
 
Greetings
Ing. Morgana
Labels (1)
0 Kudos
Reply
1 Reply

1,029 Views
Alban
Senior Contributor II
Hello,

I am afraid that you are unlikely to receive feedback from your schematics as it is in a quality that does not allow characters to be read.

Cheers,
Alban.
0 Kudos
Reply