MC13213 and BeeStack Low Power Module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC13213 and BeeStack Low Power Module

2,163件の閲覧回数
Spell
Contributor I
Hi guys,

I'm starting to use the Low Power library in MAC codebase but I have a problem.

When I call one radio interface functions like PWRLib_RadioDozeReq or PWRLib_RadioAcomaDozeReq I'm not able to set the radio modem in Acoma or Doze state because both functions returns always an error...

Do you have any suggestion to me?

regards,
Filippo
ラベル(1)
0 件の賞賛
返信
1 返信

999件の閲覧回数
Mads
Contributor V
Spell,
 
if you look at these functions you will see that they call the low power functions in the MAC.
the MAC will return not sucess in case the MAC does not allow you to go to sleep.
 
the typical scenario is that your device is a RxOnWhenIdle device (e.g. a coordinator or router)
and not a polling end device. in this case you will not be allowed to sleep.
 
Please look at the 802.15.4 reference manual for details about these functions, and take a look at the MyStarNetwork demo that utilized the power lib.
 
BR,
Mads
0 件の賞賛
返信