C Code request for ASK Transceiver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

C Code request for ASK Transceiver

1,798 Views
ILEY
Contributor I
I need a C code to use a  ASK Transceiver , i am using in the TX a timer interrupt to put a data, in the rx timer an input capture to catch a start bit, and then a other timer to sample 4 times for bit. But i have problems with RF interference.
 
may i help me?
 
thanks.


--
Alban Edit: subject line corrected



Message Edited by Alban on 2007-10-15 11:09 PM
Labels (1)
0 Kudos
Reply
1 Reply

1,138 Views
UK_CF_FAE
NXP Employee
NXP Employee
Which microcontroller?
0 Kudos
Reply