MC13213 and BeeStack Low Power Module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC13213 and BeeStack Low Power Module

2,194 次查看
Spell
Contributor I
Hi guys,

I'm starting to use the Low Power library in MAC codebase but I have a problem.

When I call one radio interface functions like PWRLib_RadioDozeReq or PWRLib_RadioAcomaDozeReq I'm not able to set the radio modem in Acoma or Doze state because both functions returns always an error...

Do you have any suggestion to me?

regards,
Filippo
标签 (1)
0 项奖励
回复
1 回复

1,030 次查看
Mads
Contributor V
Spell,
 
if you look at these functions you will see that they call the low power functions in the MAC.
the MAC will return not sucess in case the MAC does not allow you to go to sleep.
 
the typical scenario is that your device is a RxOnWhenIdle device (e.g. a coordinator or router)
and not a polling end device. in this case you will not be allowed to sleep.
 
Please look at the 802.15.4 reference manual for details about these functions, and take a look at the MyStarNetwork demo that utilized the power lib.
 
BR,
Mads
0 项奖励
回复