MC13213 & SMAC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC13213 & SMAC

2,397 次查看
Anani
Contributor I
Hi,
 
I am using one of the SMAC demo applications to test my custom board with MC13213. It looks like reading from any of the modem registers (SPI singular transaction) gives back 0x0000!?! The writing should work, because I am able to change the CLKO from the default after modem reset 32.78....KHz to 8MHZ (this only can be done by successful write to the 0x0A register). Of cause I can suspect my hardware, but then why the writing works?
 
Any ideas....
 
Thank you!
标签 (1)
0 项奖励
回复
2 回复数

817 次查看
RedMountain
Contributor I
It may be possible that you have shorted the MISO pin to ground, or that you are applying some sort of loading to that pin. I, too, have had some trouble with a custom board and the MC1321x. I think a lot of it had to do with loading the test pins, although my results were somewhat sporadic. Sometimes I could look at the serial communication between the modem and mcu, other times I couldn't. The clincher for me was figuring out that on one of my boards, by loading the IRQ pin with the scope, I flatlined all the other SPI lines. Do you have test points for the test pins on the MCU? The MC1321x reference manual doesn't tell you what they correspond to (merely saying that you're not supposed to connect them. Another hint, I think), but they are, as found in a reference design provided by Freescale:

Pin 65: PTE5/SPICLK
Pin 66: PTE4/MOSI
Pin 67: PTE3/MISO
Pin 68: PTE2/CE_B
Pin 69: IRQ/IRQ
Pin 70: PTD1/RXTXEN
Pin 71: PTD3/RST_B

Do you have another board that you could try SMAC on?

Hope that helps.
0 项奖励
回复

817 次查看
kingking
Contributor I

hello,how can i get mc13213 SMAC demo applications? Where did you download the code?Could you help me,friend?

0 项奖励
回复