MC13192 Rf Receive IRQ Interrupt with CRC NOT valid

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC13192 Rf Receive IRQ Interrupt with CRC NOT valid

1,760 次查看
LakeRat
Contributor I
Is there anyway to control the occurrence rate of the IRQ Receive Interrupt where the CRC is NOT valid. Is there some hidden register to control this spurious Receive Interrupt. I see this on the SARD card hardware with the latest SMAC code. I see this same rate of occurrence on other hardware designs even when I put the MC13192 based Hardware into an RF chamber... NO outside 2.4G Band Signals.
This interrupt happens randomly sometimes 2 or 3 times in 5 a second window.  
标签 (1)
0 项奖励
回复
1 回复

1,217 次查看
GusPS
Contributor I

Nice question. I'm facing the same situation. Did you find a solution?

0 项奖励
回复