MC13192 Rf Receive IRQ Interrupt with CRC NOT valid

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC13192 Rf Receive IRQ Interrupt with CRC NOT valid

1,841件の閲覧回数
LakeRat
Contributor I
Is there anyway to control the occurrence rate of the IRQ Receive Interrupt where the CRC is NOT valid. Is there some hidden register to control this spurious Receive Interrupt. I see this on the SARD card hardware with the latest SMAC code. I see this same rate of occurrence on other hardware designs even when I put the MC13192 based Hardware into an RF chamber... NO outside 2.4G Band Signals.
This interrupt happens randomly sometimes 2 or 3 times in 5 a second window.  
ラベル(1)
0 件の賞賛
返信
1 返信

1,298件の閲覧回数
GusPS
Contributor I

Nice question. I'm facing the same situation. Did you find a solution?

0 件の賞賛
返信