M9S08QG8 development board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M9S08QG8 development board

ソリューションへジャンプ
3,550件の閲覧回数
miguelangelferr
Contributor II

Hi People.

Currently I want to use the demo board DEMO9S08QG8 from  development board, I use IDE Codewarrior V 6.3 with no problem with FL16 Microcontroller, and others boards, however this board has no communication with my codewarrior.

I could discover that this demo board DEMO9S08QG8 is under "Multilink USB 2.0" in the devices config list whn I connect it to my computer through and USB cable, so I believe there is a misunderstanding between the DEMO9S08QG8 board and my Windows 10 because of wrong assigned drivers.

 

Can you help me with the proper drivers for the DEMO9S08QG8 board, or maybe you can show me another flash prgramming board, as I have developed my application already, What I need is to load the s19 file into the flash of microcontroller.

Thanks!

タグ(1)
0 件の賞賛
返信
1 解決策
3,536件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

We do not recomment to use codewarrior 6.3 any more, this is no longer supported, I recommend you that change to codewarrior 11.1

 

Also can you try to use the tools from P&E and the end the DEMO9S08QG8 has a OSBM on it

 

 

https://www.pemicro.com/osbdm/

regards

Vicente

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,537件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

We do not recomment to use codewarrior 6.3 any more, this is no longer supported, I recommend you that change to codewarrior 11.1

 

Also can you try to use the tools from P&E and the end the DEMO9S08QG8 has a OSBM on it

 

 

https://www.pemicro.com/osbdm/

regards

Vicente

 

0 件の賞賛
返信