PN532 Sector blocks programming HELP!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532 Sector blocks programming HELP!

2,185 Views
furkanyerlikaya
Contributor I

Hello, we bought a board with this module, but there is a problem, can you help?
PN532 How to write RFID coded data blocks (Sector Blocks) to RFID card?
When we look at the internet, we see libraries over NFC,
but we want to program the sector blocks from the RFID library (for 1k Mifare Card) with RFID,
how can we program it? I will be glad if you can help, have a nice day.

0 Kudos
Reply
1 Reply

2,162 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the related information as the thread.

URL:https://community.nxp.com/t5/NFC/PN532-Plug-n-Play-to-PC-Win-or-Linux/m-p/834343.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply