LVD Detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVD Detection

Jump to solution
2,361 Views
chetan
Contributor I

i want to know how to generate LVD interrupt from bean inspector in  MC9S08PT16

Labels (1)
Tags (4)
1 Solution
2,212 Views
arpitaagarwal-b
NXP Employee
NXP Employee

Hello Chetan,

LVD Interrupt can be enabled in CPU bean (once the PE is enabled in the project, no need to add any other bean) from the options available in component inspector. To see the list of the options switch to "Expert" view (circled in the image below) of the inspector. Go to Internal Peripherals-->LVD Module-->LVW interrupt to enable the interrupt.

LVD_PT16.png

View solution in original post

0 Kudos
Reply
3 Replies
2,213 Views
arpitaagarwal-b
NXP Employee
NXP Employee

Hello Chetan,

LVD Interrupt can be enabled in CPU bean (once the PE is enabled in the project, no need to add any other bean) from the options available in component inspector. To see the list of the options switch to "Expert" view (circled in the image below) of the inspector. Go to Internal Peripherals-->LVD Module-->LVW interrupt to enable the interrupt.

LVD_PT16.png

0 Kudos
Reply
2,212 Views
chetan
Contributor I

Dear Arpita

Thanks a lot arpita

Problem solved I don’t know to see it in "Expert" view

Best Regards,

Chetan Namjoshi

2,212 Views
Monica
Senior Contributor III

Hello Chetan!

I ran into this document, maybe it has the info you need MC9S08PT16 Reference Manual

Hope it helps!

Regards,

Monica.

0 Kudos
Reply