LTIB is showing error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB is showing error

1,735 Views
admin
Specialist II

Hello, I am trying to install gstreamer codec in IMX51 board. for that i downloaded onr document from website.  I folloed the steps accourding to that document. In that when i tried to install LTIB by giving command ./ltib. It is not working. All other things are fine. I copies all the things in /opt and i replaced the spec files. Now my error is  [code]ariem@ariem-desktop:~/Desktop/plugins/L2.6.28_4.5.1_SDK_Aug2009_source/ltib$ ./ltib
sh: tclsh: command not found

ltib cannot be run because one or more of the host packages needed to run it
are either missing or out of date or not in ltib's standard path. Please
install/upgrade these packages on your host. If you have your own utilities
in non-standard paths, please add an entry into the .ltibrc file for example:

%path_std
/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes

Package Minimum ver Installed info
------- ----------- ---------------
zlib-devel 0 not installed
rpm 0 not installed
rpm-build 0 not installed
m4 0 not installed
bison 0 not installed
tcl 0 not installed

Died at ./ltib line 1397.
traceback:
main::host_checks:1397
main:542


Started: Tue Dec 22 18:54:26 2009
Ended: Tue Dec 22 18:54:27 2009
Elapsed: 1 seconds


Build Failed

Exiting on error or interrupt
ariem@ariem-desktop:~/Desktop/plugins/L2.6.28_4.5.1_SDK_Aug2009_source/ltib$
[/code]

Labels (1)
0 Kudos
Reply
1 Reply

1,051 Views
peg
Senior Contributor IV

Hello Sharief,

 

The appropriate forum for discussion of this product is the "Other Microcontrollers/Microprocessors" forum. You will find more help there than in this 8-bit forum. Expect the two threads you have started to be moved there soon.

 

0 Kudos
Reply