JM60 internal osc problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JM60 internal osc problem

2,092 次查看
donw
Contributor IV

Hi all

I have a 908JM60 which is initilised with the code below, so the internal osc gives a bus ~8mhz

This work fine, until I try to call the code again while running, if which case it loops on the while_Cpu0

(ie the lock bit is never set)

What is wrong?

 

      sei      
        ; MCGC2: BDIV=1,RANGE=0,HGO=0,LP=0,EREFS=0,ERCLKEN=0,EREFSTEN=0
        MOV     #$040,MCGC2             ; Set MCGC2 register
        ; MCGC1: CLKS=0,RDIV=0,IREFS=1,IRCLKEN=1,IREFSTEN=0
        MOV     #$06,MCGC1             ; Set MCGC1 register
        ; MCGC3: LOLIE=0,PLLS=0,CME=0,VDIV=1
        MOV     #$01,MCGC3             ; Set MCGC3 register
while_Cpu0:                            ; Wait until FLL is locked
         BRCLR   6,MCGSC,while_Cpu0
        cli

       rts

标签 (1)
0 项奖励
回复
2 回复数

1,513 次查看
yzhou
Contributor I

Hi donw,

Is it possible caused by your calling this routine in order to switch from PEE mode to FEI mode, which is not a standard method for mode switching?

 

Thanks,

Zhou

0 项奖励
回复

1,513 次查看
donw
Contributor IV

The problem seems to occur when changing back from an external xtal mode, which has

MOV     #$046,MCGC2             ; Set MCGC2 register

 

so long as the code above has

MOV     #$040,MCGC2             ; Set MCGC2 register

and not

MOV     #$046,MCGC2             ; Set MCGC2 register

then it works OK.

Not sure what the bit feild EREFS really does..

 

0 项奖励
回复