Is possible to program a MC9S08GT60CFB with USB-ML-MON08?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is possible to program a MC9S08GT60CFB with USB-ML-MON08?

Jump to solution
2,710 Views
TG
Contributor I

Hello everybody.

 

I want to know if it's possible to program/debug a MC9S08GT60CFB device with a USB-ML-MON08 interface. I think that the answer is no, but i don't know if exists any adapter or something like that to make it possible.

 

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
1,743 Views
peg
Senior Contributor IV

Hello and welcome to the fora, TG,

 

Your USB-ML-MON08 is only good for HC08 devices (i.e. one that use a MON08 interface)

 

You will  need a USB-ML-12 or similar BDM type adapter to programme S08 devices (one of which is the 9S08GT60)

 

You might also consider an OSBDM as discussed in the community project forums here.

 

Message Edited by peg on 2009-07-16 07:37 AM

View solution in original post

0 Kudos
Reply
2 Replies
1,744 Views
peg
Senior Contributor IV

Hello and welcome to the fora, TG,

 

Your USB-ML-MON08 is only good for HC08 devices (i.e. one that use a MON08 interface)

 

You will  need a USB-ML-12 or similar BDM type adapter to programme S08 devices (one of which is the 9S08GT60)

 

You might also consider an OSBDM as discussed in the community project forums here.

 

Message Edited by peg on 2009-07-16 07:37 AM
0 Kudos
Reply
1,743 Views
TG
Contributor I

Ok, thanks for your help and the fast reply peg.

 

0 Kudos
Reply