Is possible to program a MC9S08GT60CFB with USB-ML-MON08?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is possible to program a MC9S08GT60CFB with USB-ML-MON08?

ソリューションへジャンプ
2,696件の閲覧回数
TG
Contributor I

Hello everybody.

 

I want to know if it's possible to program/debug a MC9S08GT60CFB device with a USB-ML-MON08 interface. I think that the answer is no, but i don't know if exists any adapter or something like that to make it possible.

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,729件の閲覧回数
peg
Senior Contributor IV

Hello and welcome to the fora, TG,

 

Your USB-ML-MON08 is only good for HC08 devices (i.e. one that use a MON08 interface)

 

You will  need a USB-ML-12 or similar BDM type adapter to programme S08 devices (one of which is the 9S08GT60)

 

You might also consider an OSBDM as discussed in the community project forums here.

 

Message Edited by peg on 2009-07-16 07:37 AM

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,730件の閲覧回数
peg
Senior Contributor IV

Hello and welcome to the fora, TG,

 

Your USB-ML-MON08 is only good for HC08 devices (i.e. one that use a MON08 interface)

 

You will  need a USB-ML-12 or similar BDM type adapter to programme S08 devices (one of which is the 9S08GT60)

 

You might also consider an OSBDM as discussed in the community project forums here.

 

Message Edited by peg on 2009-07-16 07:37 AM
0 件の賞賛
返信
1,729件の閲覧回数
TG
Contributor I

Ok, thanks for your help and the fast reply peg.

 

0 件の賞賛
返信