Is it possible to copy the contents of one controller to another

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to copy the contents of one controller to another

1,985 Views
matrixmm
Contributor I
Hi, sorry for the stupid question.
Is it possible to copy the contents of one controller to another.
I have the same two boards. One is working and second broken. I repaired the second board and replace burned HCS08 controler with new one.
The question is, can I somehow copy the content from a working controller to a clean one?
using USBDM for example?
any help will be appreciated
0 Kudos
Reply
3 Replies

1,936 Views
matrixmm
Contributor I

I solved. If someone has a similar problem, it can be easily done using USBDM Memory dump. Rip flash to a file and upload with FlashProgrammer to a new chip.

0 Kudos
Reply

1,970 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

 

If the original firmware is not protected, yes you can perform an "attach" on CodeWarrior using the multilink.

 

0 Kudos
Reply

1,943 Views
matrixmm
Contributor I

I try program one chip and clone to another. Just for learning.
It's not protected. In codewarrior i choose MAC Tools -> Attach to target. But not have USBD programmer to choose. :(. Whats i do wrong?
Any help will be apreciated.

 

attache.jpg

0 Kudos
Reply