Is it necessary to register CodeWarrior Special Edition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it necessary to register CodeWarrior Special Edition

2,521 Views
robert2000
Contributor II
Hello
I download CodeWarrior Special edition for HC(S)08 /ColdfireV1 Version 6.2. This a free software but the software is requesting to Register. I don't understand what I should do.
Thanks for your help
Labels (1)
0 Kudos
Reply
4 Replies

1,330 Views
NLFSJ
Contributor III
The special edition licenses do not require registration.   They are active upon installation. 
Have you placed the license.dat file in the directory where you installed the software?
0 Kudos
Reply

1,330 Views
robert2000
Contributor II
HelloNina
I am able to access the software which is working well. But it's time limited: only one month.
I am not sure to understand your comment but I give the same directory for the installation and 
the license.dat file . Is that correct?
Robert
0 Kudos
Reply

1,330 Views
J2MEJediMaster
Specialist I
We've had a glitch where people are getting the Evaluation Edition of the CodeWarrior software when they download the Special Edition. The Evaluation edition is similar to the Special Edition, except that it's fully featured for one month. Once the trial period ends, it becomes the Special Edition, with its code size limits. See FAQ-28561 for a little more detail. And no, you don't have to register the software, unless you want to purchase the full features after the temporary license expires.

---Tom
0 Kudos
Reply

1,330 Views
robert2000
Contributor II
Hello Tom
 
Thanks a lot for this info.
So , I have just to keep the software and, I will get the special Edition after one month.
 
Best Regards
Robert
0 Kudos
Reply