ICDHCS08 & Win7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ICDHCS08 & Win7

1,418 Views
tonyp
Senior Contributor II

Hi all,

 

I've already made a support request to P&E but since I'm in the middle of an urgent project, and I need to get this working asap.

 

Due to a PC replacement (old is malfunctioning, so I can no longer use it) I went from WinXP to Win7 (no choice, as WinXP is no longer available.)

 

Attempting to re-install ICDHCS08 gives several errors and aborts installation.  P&E's response as for the availability of an update is pending.  But, I need to work.  So, has anyone managed to get this program to run under Win7?

 

(Copying the raw files from a backup -- no installation -- seems to run but fails to see the Cyclone PRO).

 

TIA

Labels (1)
0 Kudos
Reply
1 Reply

1,247 Views
Designer11
Contributor IV

Tony,

 

I am not familiar with the program. But, you can  try to run the program in Windows XP mode under Windows Virtual PC

0 Kudos
Reply