How to calculate the oscillator capacitor value for a switched capacitor (MAX7405)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to calculate the oscillator capacitor value for a switched capacitor (MAX7405)?

722件の閲覧回数
lucylin
Contributor I

Hello, everyone!

I am thinking of  using an 8-order LPF switched capacitor: MAX7405 http://www.kynix.com/Detail/407475/MAX7405ESA%2B.html

The cut-off frequency should be set by simply connecting an external oscillator capacitor, Cosc.

I would like to design a 50Hz cut-off frequency but I have doubts on my calculation for the given formula in the datasheet.

max7405 datasheet

Since I want to have a 50Hz fC, I needs the fCLK to be 5000Hz

From the given equation:

fOSC(kHz) = (K * 10^3) / Cosc; Cos in pF , K = 34 for max7405 
5000(k) = (34 * 10^3) / ( C * 1pF)
5000 = 34 / ( C * 1pF) 
C = 34 / 5nF 
C = 6800M 

By using the above equation, I calculated an extreme large capacitor with Mega value which is not reasonable.

Am I calculating it in the right way?

Best regards,

Lucy Lin
ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)