How to AND the accumulator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to AND the accumulator

ソリューションへジャンプ
2,185件の閲覧回数
theGhost
Contributor I

Hello,

 

I have a GT16A, HCSO8 familly.

I want to AND the accumulator.

 

ANDing two ports is easy. eg: AND PTAD, PTBD

 

But How do you AND the accunulator with a value (eg: #$AA) or with value in memory or with a port?

 

Thank you for your help.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,016件の閲覧回数
peg
Senior Contributor IV

Hello the Ghost,

 

The AND instruction ALWAYS AND's with the accumulator!

The example you show is not valid.

One way to perform your example is:

 

LDA PTAD

AND PTBD

 

Your other question would be:

 

LDA #$AA

AND PTAD

 

Here is the instruction from the manual:

AND Logical AND ANDOperation A ← (A) & (M)Description Performs the logical AND between the contents of A and the contents ofM and places the result in A. Each bit of A after the operation will be thelogical AND of the corresponding bits of M and of A before the operation.Condition Codesand BooleanFormulae:V: 0ClearedN: R7Set if MSB of result is 1; cleared otherwiseZ: R7&R6&R5&R4&R3&R2&R1&R0Set if result is $00; cleared otherwiseSource Forms,AddressingModes, MachineCode, Cycles, andAccess DetailsV H I N Z C0 1 1 — — ↕ ↕ —SourceFormAddr.ModeMachine Code HCS08CyclesAccessOpcode Operand(s) DetailAND #opr8i IMM A4 ii 2 ppAND opr8a DIR B4 dd 3 rppAND opr16a EXT C4 hh ll 4 prppAND oprx16,X IX2 D4 ee ff 4 prppAND oprx8,X IX1 E4 ff 3 rppAND ,X IX F4 3 rfpAND oprx16,SP SP2 9ED4 ee ff 5 pprppAND oprx8,SP SP1 9EE4 ff 4 prppFreescale Semiconductor, IFreescale Semiconductor, Inc.For More Information On This Product,Go to: www.freescale.comnc

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,016件の閲覧回数
rocco
Senior Contributor II

Hi Ghost,

 

You misunderstand, " AND PTAD, PTBD" is not a valid instruction in the S08. It should be giving you a syntax error.

 

The AND instruction ONLY works with the accumulator. To AND the immediate value $AA to the accumulator, the instruction would be " AND #$AA". To AND the contents of memory to the accumulator, the instruction would be "AND <address>", regardless of whether <address> is flash, ram or a port. There is no instruction to AND directly to memory or a port.

 

----

 

Oops: I see Peg and I cross-posted.

0 件の賞賛
返信
2,017件の閲覧回数
peg
Senior Contributor IV

Hello the Ghost,

 

The AND instruction ALWAYS AND's with the accumulator!

The example you show is not valid.

One way to perform your example is:

 

LDA PTAD

AND PTBD

 

Your other question would be:

 

LDA #$AA

AND PTAD

 

Here is the instruction from the manual:

AND Logical AND ANDOperation A ← (A) & (M)Description Performs the logical AND between the contents of A and the contents ofM and places the result in A. Each bit of A after the operation will be thelogical AND of the corresponding bits of M and of A before the operation.Condition Codesand BooleanFormulae:V: 0ClearedN: R7Set if MSB of result is 1; cleared otherwiseZ: R7&R6&R5&R4&R3&R2&R1&R0Set if result is $00; cleared otherwiseSource Forms,AddressingModes, MachineCode, Cycles, andAccess DetailsV H I N Z C0 1 1 — — ↕ ↕ —SourceFormAddr.ModeMachine Code HCS08CyclesAccessOpcode Operand(s) DetailAND #opr8i IMM A4 ii 2 ppAND opr8a DIR B4 dd 3 rppAND opr16a EXT C4 hh ll 4 prppAND oprx16,X IX2 D4 ee ff 4 prppAND oprx8,X IX1 E4 ff 3 rppAND ,X IX F4 3 rfpAND oprx16,SP SP2 9ED4 ee ff 5 pprppAND oprx8,SP SP1 9EE4 ff 4 prppFreescale Semiconductor, IFreescale Semiconductor, Inc.For More Information On This Product,Go to: www.freescale.comnc

 

0 件の賞賛
返信