Help with Graphical LCD 122*32 - MC9S08DN60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help with Graphical LCD 122*32 - MC9S08DN60

2,474件の閲覧回数
Tidum
Contributor I
hi all
i'm using MC9S08DN60 to drive a Graphical lcd module 122*32.
well i've tried all possible ways to turn on a pixel but i'm not getting help.
i'm uploading my code and the datasheet of the lcd on to the forum.
thanks in advance
 
 
 
 
 
 
 
Added p/n to subject.



Message Edited by NLFSJ on 2008-09-03 10:59 PM

 

main2.c

YG_12232B_SBGB_F_B_SPEC_b01.pdf

Message Edited by t.dowe on 2009-10-27 12:11 PM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,308件の閲覧回数
jag
Contributor IV
Hi,
I never used your display, but from a very fast read of the datasheet I think it should work like another dislpay (alphanumeric, 2 lines, 8 char per line) I'm using right now: it's a display with a KS 0066 controller.
Check the datasheet of the KS0066, it should give you some hint how to use yours.

Bye Jack
0 件の賞賛
返信

1,308件の閲覧回数
Scott134
Contributor II
I have been caught by this before - make sure the contrast pot is set correctly.  The display may be working and you can't see it.
 
Scott
0 件の賞賛
返信