Help with Graphical LCD 122*32 - MC9S08DN60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help with Graphical LCD 122*32 - MC9S08DN60

2,458 Views
Tidum
Contributor I
hi all
i'm using MC9S08DN60 to drive a Graphical lcd module 122*32.
well i've tried all possible ways to turn on a pixel but i'm not getting help.
i'm uploading my code and the datasheet of the lcd on to the forum.
thanks in advance
 
 
 
 
 
 
 
Added p/n to subject.



Message Edited by NLFSJ on 2008-09-03 10:59 PM

 

main2.c

YG_12232B_SBGB_F_B_SPEC_b01.pdf

Message Edited by t.dowe on 2009-10-27 12:11 PM
Labels (1)
0 Kudos
Reply
2 Replies

1,292 Views
jag
Contributor IV
Hi,
I never used your display, but from a very fast read of the datasheet I think it should work like another dislpay (alphanumeric, 2 lines, 8 char per line) I'm using right now: it's a display with a KS 0066 controller.
Check the datasheet of the KS0066, it should give you some hint how to use yours.

Bye Jack
0 Kudos
Reply

1,292 Views
Scott134
Contributor II
I have been caught by this before - make sure the contrast pot is set correctly.  The display may be working and you can't see it.
 
Scott
0 Kudos
Reply