Help: MMDS05 fail to load firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help: MMDS05 fail to load firmware

2,873件の閲覧回数
admin
Specialist II
I am using the MMDS05 and M68EM08 series emulator modules, but now when I try to load ZAP MMDS 6808, it always fails to load firmware, I mean it always reports "loading firmware"? Is there any possible root cause that I can try to fix?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,882件の閲覧回数
rocco
Senior Contributor II
Hi, Simon:

Is your target powered up and is it's clock running?

The clock in my system is configured to run from the target, which I believe is the default. If the target is not providing a clock to the processor, my system hangs at the "Loading Firmware" message.
0 件の賞賛
返信

1,882件の閲覧回数
admin
Specialist II
Hi, rocco:
 
I replaced the target MCU and it work now. I think maybe the target has some problem.
Thanks for your advice.
0 件の賞賛
返信