Help: MMDS05 fail to load firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help: MMDS05 fail to load firmware

2,338 次查看
admin
Specialist II
I am using the MMDS05 and M68EM08 series emulator modules, but now when I try to load ZAP MMDS 6808, it always fails to load firmware, I mean it always reports "loading firmware"? Is there any possible root cause that I can try to fix?
标签 (1)
0 项奖励
回复
2 回复数

1,347 次查看
rocco
Senior Contributor II
Hi, Simon:

Is your target powered up and is it's clock running?

The clock in my system is configured to run from the target, which I believe is the default. If the target is not providing a clock to the processor, my system hangs at the "Loading Firmware" message.
0 项奖励
回复

1,347 次查看
admin
Specialist II
Hi, rocco:
 
I replaced the target MCU and it work now. I think maybe the target has some problem.
Thanks for your advice.
0 项奖励
回复