HCS08 already programmed and temperature range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS08 already programmed and temperature range

1,985件の閲覧回数
franticcarlitos
Contributor II

First question

S08JM60 microcontrollers are orderable already programmed (with firmware that let me to use it for jtag programming of another kinetics mcu)? Is there any parameter key in buy code that let me know this thing?

 

Second question

Is there any mcu of this family that has -40°:+105° temperature range?

 

Thanks

ラベル(1)
2 返答(返信)

1,867件の閲覧回数
Monica
Senior Contributor III

Hello Frantic Carlitos,

Were these answers helpful? Please keep us posted! :smileywink:

Best regards,

Monica

0 件の賞賛
返信

1,867件の閲覧回数
Joel69003
Contributor IV

Hi Frantic,

If you buy the microcontroller, it will be blank. Maybe you want to build your own USBDM ? In this case have a look to S08JS16 versions which can be flashed throw the USB connection. It is also possible to buy USBDM on eBay for example.

To answer you second question, no. S08JM devices are only available from -40°C to 85°C.

Regards,

Joel Guittet