HCS08 already programmed and temperature range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS08 already programmed and temperature range

2,037 Views
franticcarlitos
Contributor II

First question

S08JM60 microcontrollers are orderable already programmed (with firmware that let me to use it for jtag programming of another kinetics mcu)? Is there any parameter key in buy code that let me know this thing?

 

Second question

Is there any mcu of this family that has -40°:+105° temperature range?

 

Thanks

Labels (1)
2 Replies

1,919 Views
Monica
Senior Contributor III

Hello Frantic Carlitos,

Were these answers helpful? Please keep us posted! :smileywink:

Best regards,

Monica

0 Kudos
Reply

1,919 Views
Joel69003
Contributor IV

Hi Frantic,

If you buy the microcontroller, it will be blank. Maybe you want to build your own USBDM ? In this case have a look to S08JS16 versions which can be flashed throw the USB connection. It is also possible to buy USBDM on eBay for example.

To answer you second question, no. S08JM devices are only available from -40°C to 85°C.

Regards,

Joel Guittet