HCS08 already programmed and temperature range

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HCS08 already programmed and temperature range

1,948 次查看
franticcarlitos
Contributor II

First question

S08JM60 microcontrollers are orderable already programmed (with firmware that let me to use it for jtag programming of another kinetics mcu)? Is there any parameter key in buy code that let me know this thing?

 

Second question

Is there any mcu of this family that has -40°:+105° temperature range?

 

Thanks

标签 (1)
2 回复数

1,830 次查看
Monica
Senior Contributor III

Hello Frantic Carlitos,

Were these answers helpful? Please keep us posted! :smileywink:

Best regards,

Monica

0 项奖励
回复

1,830 次查看
Joel69003
Contributor IV

Hi Frantic,

If you buy the microcontroller, it will be blank. Maybe you want to build your own USBDM ? In this case have a look to S08JS16 versions which can be flashed throw the USB connection. It is also possible to buy USBDM on eBay for example.

To answer you second question, no. S08JM devices are only available from -40°C to 85°C.

Regards,

Joel Guittet