HCS08 Unleashed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS08 Unleashed

17,861 Views
fabio
Contributor IV
Hello folks!

My book is finally ready and I would like to share the news with you. The final title is: "HCS08 Unleashed: Designer's Guide to the HCS08 Microcontrollers".



It is a mix of a reference book and a hands-on course. Through the 412 pages, many interesting topics are covered, such as: the HCS08 CPU architecture, programmer's model, peripherals,etc.

The first chapters cover the basics of the architecture, the Codewarrior tool and a quick C review (yes, the book is focused on C development).

There are over 70 examples and listings (including some small applications in the last chapter). I hope you like it. The table of contents and the example files can be downloaded at: www.sctec.com.br/hcs08 .

I hope the book is available for purchase in about two weeks (some issues were detected in the proof copy and I had to start the publishing process from the beginning) through Booksurge ( www.booksurge.com ) and later through Amazon ( www.amazon.com ). As soon as the book is available, I'll let you know (and I would love to hear any comments!).

Best regards,
Labels (1)
0 Kudos
Reply
17 Replies

8,892 Views
fanbanlo
Contributor I
Which dev kit should I buy along with this book to follow the example? thanks.
0 Kudos
Reply

8,892 Views
fabio
Contributor IV

Most examples were designed to run on the DEMO9S08QG8, but there is also examples for the DEMOQE board, DEMO9S08AW60E, M68DEMO908GB60 and DEMO9S08LC60.

 

Best regards,

0 Kudos
Reply

8,892 Views
fanbanlo
Contributor I

DEMO9S08QG8 is "No Longer Manufactured" : http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMO9S08QG8&tab=Buy_Parametric_Tab&cl...

 

Is DEMO9S08QG8E ok? Or which one should I purchase?  Thank you.

0 Kudos
Reply

8,892 Views
fabio
Contributor IV

I think it is basically the same kit.

 

Best regards,

0 Kudos
Reply

8,892 Views
mimmo69
Contributor I

Thank you very much!!!

 

I continue to have problems with your web site, but may be it is a problem to my connection.

 

Is there another place where I can find the material of the book?

 

Best regards,

 

mimmo

0 Kudos
Reply

8,892 Views
fabio
Contributor IV

Hi Mimmo,

 

Unfortunatelly, there is no other place where you can download the files. You can email me and I will send any files you need.

 

f a b i o [at] s c t e c [dot] c o m [dot] b r

 

Best regards,

 

0 Kudos
Reply

8,892 Views
jagged
Contributor I

Hello Fabio,

 

I purchased your book a while ago and it is very good & useful.

Thanks for putting the time in to providing such excellent content into one great book.

 

Now I would very much like to make use of the online content & files but have encountered some problems.

 

Like mimmo, I am having problems accessing the download files from your site: www.sctec.com.br/hcs08.

 

Here is the response I am seeing:

 

Warning: require_once() [function.require-once]: open_basedir restriction in effect. File(/home/httpd/html/sctec.com.br/html//includes/version.php) is not within the allowed path(s): (/home/httpd/vhosts/sctec.com.br/httpdocs:/tmp) in /home/httpd/vhosts/sctec.com.br/httpdocs/includes/mambo.php on line 41 

Fatal error: require_once() [function.require]: Failed opening required '/home/httpd/html/sctec.com.br/html//includes/version.php' (include_path='.:/usr/local/lib/php') in /home/httpd/vhosts/sctec.com.br/httpdocs/includes/mambo.php on line 41

 

 

Any help would be appreciated.

 

Best regards,

Michael

0 Kudos
Reply

8,892 Views
fabio
Contributor IV

Hi Jagged,

 

The website is working  again!

 

Besg regards and a great 2010!

0 Kudos
Reply

8,892 Views
jagged
Contributor I

Fabio,

 

I just read your response to my site access problem. Thank you so much for making your site accessible! - I have now downloaded the relevant chapter files that I was planning to run on my demo9s08qg8 module.

This extra material provides very useful support for the actual book!

 

Best regards to you as well.

 

Michael

0 Kudos
Reply

8,892 Views
admin
Specialist II

I bought your book fabio. Arrived yesterday but so far I haven't had a chance to do anything but flip thru the pages. So far, it looks good and appears to have everything about the S08 all together in one place.

 

Nice work. 

0 Kudos
Reply

8,892 Views
mimmo69
Contributor I

Hi Fabio.

 

Thanks a lot for your book!!! It's a good way to learn HCS08 uC.

 

I have a problem.

 

I have problem with connection to your site: www.sctec.com.br/hcs08

 

I need to download the file: hcs08.h.

 

Can you help me?

 

Best regards,

 

mimmo

0 Kudos
Reply

8,891 Views
fabio
Contributor IV

Hi Mimmo,

 

The webpage is working ok for me. What kind of problem are you experiencing?

 

The attached file include the examples for chapter 13, all of them also include the file you need.

 

Best regards,

Message Edited by fabio on 2009-11-09 10:23 AM
Message Edited by t.dowe on 2009-11-09 10:12 AM
0 Kudos
Reply

8,892 Views
Denn
Contributor I
Hello Fabio,
 
Congratulations for your new book on HCS08 controllers.Hope this would be a good reference for the folks working on them.
 
Regards,
Denn


Message Edited by Denn*** on 2008-03-07 06:18 AM
0 Kudos
Reply

8,892 Views
J2MEJediMaster
Specialist I
Congratulations, fabio! I understand what you went through...I published a book on Power Macintosh Programming on how to use the (then new) PowerPC back in 1994. It was a lot of work, talking about the microarchitecture, and then coming up with some code examples that were simple enough to be instructive, yet sophisticated enough to do something practical.  Again, great job. I know you're glad that the writing part is over. I hope it becomes a bestseller, or at least the royalty checks are fabulous.

---Tom


Message Edited by J2MEJediMaster on 2008-03-11 12:23 PM
0 Kudos
Reply

8,892 Views
fabio
Contributor IV
Hi Denn and Tom,

Thank you for your kindly words. I am very anxious to see the real book. I hope it be useful for everybody.

Tom:

Wow, PowerPC, very cool. Back 1994 ? Even more cool. I have read some texts about the architecture (mostly the PPC604), but I must admit it is light years from me. Today, the most advanced machines I use to program are ARMs (ARM7 and Cortex-M3).

Best regards and thanks again!
0 Kudos
Reply

8,892 Views
fabio
Contributor IV
The book is available at Amazon.com:

Best regards,


Message Edited by fabio on 2008-03-28 02:46 PM
0 Kudos
Reply

8,892 Views
fabio
Contributor IV
Hello everybody!

There is an errata document for some errors and smaller issues found in the book.

Right now I would like to thank CompilerGuru for pointing out most of them.

I am looking forward to find new errors (and to hear of them) so that the book gets improved more and more.

The errata can be found in the book page at www.sctec.com.br/hcs08

Thank you all!
0 Kudos
Reply