HC08 and HCS08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HC08 and HCS08

3,395 次查看
TMirnik
Contributor I

What is the difference between HC08 and HCS08 families?

标签 (1)
0 项奖励
回复
3 回复数

1,924 次查看
Klined
Contributor I

From a developer's standpoint, HC08's MON08 interface can be a real pain compared to the HCS08's BDM interface.  As stated, HCS08 is far superior.

 

0 项奖励
回复

1,924 次查看
rocco
Senior Contributor II

Also from a developer's standpoint, HCS08's BDM interface can be a real pain compared to the HC08's MMDS emulator.  As stated, the HCS08 is still superior.

0 项奖励
回复

1,924 次查看
peg
Senior Contributor IV

Hello and welcome to the fora.

 

Simply put HCS08 (or S08) is a later updated version of the HC08.

Here is an application note about it.

If you know little about either I would suggest you simply forget HC08 ever existed and just look at the S08.

S08 is always better, cheaper and most of the HC08's are dying off.

0 项奖励
回复