HC08 and HCS08

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HC08 and HCS08

4,208 Views
TMirnik
Contributor I

What is the difference between HC08 and HCS08 families?

Labels (1)
0 Kudos
Reply
3 Replies

2,737 Views
Klined
Contributor I

From a developer's standpoint, HC08's MON08 interface can be a real pain compared to the HCS08's BDM interface.  As stated, HCS08 is far superior.

 

0 Kudos
Reply

2,737 Views
rocco
Senior Contributor II

Also from a developer's standpoint, HCS08's BDM interface can be a real pain compared to the HC08's MMDS emulator.  As stated, the HCS08 is still superior.

0 Kudos
Reply

2,737 Views
peg
Senior Contributor IV

Hello and welcome to the fora.

 

Simply put HCS08 (or S08) is a later updated version of the HC08.

Here is an application note about it.

If you know little about either I would suggest you simply forget HC08 ever existed and just look at the S08.

S08 is always better, cheaper and most of the HC08's are dying off.

0 Kudos
Reply