Free Master Poll();

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Free Master Poll();

1,701 Views
leang
Contributor II

Hi dears,

When i use FMSTR_Poll();

Dose FMSTR_Poll(); have to be executed twice to output correct results?

Well  i mean ,in the while(1)   ,the program have been executed once ,and the FMSTR_Poll() also  have been executed once. Will the value of the observation variable be transferred to the Freemaster ?

Because  when i was debugging the program i  found that ,for  the first time the  Poll  is  dealing with receiving data and decoding  and something, and the second time it will transmit data.

0 Kudos
Reply
1 Reply

1,675 Views
vicentegomez
NXP TechSupport
NXP TechSupport

 Normally when you are using Free master you do not need to debug, please check the following application note

 

https://www.nxp.com/webapp/Download?colCode=AN4752

 

 

0 Kudos
Reply