For MC9S08AW16 use flash beyond 16K

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

For MC9S08AW16 use flash beyond 16K

974 次查看
rohitb
Contributor I

For MC9S08AW16 is it possible to extend the flash beyond 16K by changing the settings in linker file?

标签 (1)
0 项奖励
回复
1 回复

597 次查看
bigmac
Specialist III

Hello, and welcome to the forum.

 

To increase the amount of flash beyond 16K, you would need to alternatively select either the 32K part of the 60K part.  The appropriate PRM file would be used, using the new project wizard to create a project with the larger device as a target.

 

Regards.

Mac

 

0 项奖励
回复