For MC9S08AW16 use flash beyond 16K

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For MC9S08AW16 use flash beyond 16K

1,304件の閲覧回数
rohitb
Contributor I

For MC9S08AW16 is it possible to extend the flash beyond 16K by changing the settings in linker file?

ラベル(1)
0 件の賞賛
返信
1 返信

927件の閲覧回数
bigmac
Specialist III

Hello, and welcome to the forum.

 

To increase the amount of flash beyond 16K, you would need to alternatively select either the 32K part of the 60K part.  The appropriate PRM file would be used, using the new project wizard to create a project with the larger device as a target.

 

Regards.

Mac

 

0 件の賞賛
返信