FSICE target CPU question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FSICE target CPU question

2,234 次查看
trproc
Contributor I
I am trying to test a program using the FSICE with CodeWarrior 3.1. When starting the debugger, it asks for the target CPU and has a list of available CPUs. I am using a MC68HC908AS60A in a 52 pin PLCC package. On some of the other CPUs listed, there are versions shown for the PLCC and the QFP packages. The AS60A is only listed once with no package shown. Does anyone have any idea whether the FSICE is loading info for the PLCC or the QFP package?

Thanks
标签 (1)
0 项奖励
回复
1 回复

1,251 次查看
Oliver
Contributor III
As far as I know the die is the same no matter what the package is. The Emulator Module uses the AS60 in the QFP package anyway to emulate your target CPU, there are just a few port pins not bonded out in the PLCC package, internally they are the same.

Best regards,

Oliver
0 项奖励
回复