FSICE target CPU question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FSICE target CPU question

2,223件の閲覧回数
trproc
Contributor I
I am trying to test a program using the FSICE with CodeWarrior 3.1. When starting the debugger, it asks for the target CPU and has a list of available CPUs. I am using a MC68HC908AS60A in a 52 pin PLCC package. On some of the other CPUs listed, there are versions shown for the PLCC and the QFP packages. The AS60A is only listed once with no package shown. Does anyone have any idea whether the FSICE is loading info for the PLCC or the QFP package?

Thanks
ラベル(1)
0 件の賞賛
返信
1 返信

1,240件の閲覧回数
Oliver
Contributor III
As far as I know the die is the same no matter what the package is. The Emulator Module uses the AS60 in the QFP package anyway to emulate your target CPU, there are just a few port pins not bonded out in the PLCC package, internally they are the same.

Best regards,

Oliver
0 件の賞賛
返信