Error when flashing program into NTM88

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error when flashing program into NTM88

3,757件の閲覧回数
nguyenhuy5997
Contributor I

When i flash program into NTM88, IDE (code warrior 11.1) throw out an error like picture attached. What are reason for this error and how can i fix it? thanks you so much. im using USB BDM 

0 件の賞賛
返信
1 返信

3,735件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Huy,

please refer to section 3.1 in the AN12523 attached. Part of the firmware flash is protected and cannot be overwritten. 

JozefKozon_0-1666077196649.pngJozefKozon_0-1666077196649.png

Please also refer to the AN13321 in the following link.

https://www.nxp.com/docs/en/application-note/AN13321.pdf

With Best Regards,

Jozef

0 件の賞賛
返信