Error when flashing program into NTM88

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error when flashing program into NTM88

4,008 Views
nguyenhuy5997
Contributor I

When i flash program into NTM88, IDE (code warrior 11.1) throw out an error like picture attached. What are reason for this error and how can i fix it? thanks you so much. im using USB BDM 

0 Kudos
Reply
1 Reply

3,986 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Huy,

please refer to section 3.1 in the AN12523 attached. Part of the firmware flash is protected and cannot be overwritten. 

JozefKozon_0-1666077196649.png

Please also refer to the AN13321 in the following link.

https://www.nxp.com/docs/en/application-note/AN13321.pdf

With Best Regards,

Jozef

0 Kudos
Reply