Does CodeWarrior 11 support MC9S08SG8?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does CodeWarrior 11 support MC9S08SG8?

Jump to solution
4,130 Views
w_lingjun
Contributor III

Hi,

When I new a bare board project in CodeWarrior 11, I can't find this MCU: MC9S08SG8 on devices interface.

So does CodeWarrior 11 support MC9S08SG8?

Best regards,

Sarah

0 Kudos
Reply
1 Solution
4,114 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I believe that the problem was on the installation, you do not have installed the S08 family, the easier solution is to reinstall Codewarrior and when you are installing it you need to select the S08 devices.

I hope this will help you

View solution in original post

0 Kudos
Reply
4 Replies
4,127 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Yes

 

vicentegomez_0-1607348148178.png

You should have it.

 

Regards

Vicente G

0 Kudos
Reply
4,121 Views
w_lingjun
Contributor III

Hi Vicente,

Thanks for your reply.

This is my CW  version page

cw11_version.png

And this is the devices select interface when new a project, there is no HCS08SG Familly.

cw11_1.png

And I and can't search any devices when input MC9S0.

cw11_0.png

Is there any update packages should I install?

 

Best regards,

Sarah

 

0 Kudos
Reply
4,115 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I believe that the problem was on the installation, you do not have installed the S08 family, the easier solution is to reinstall Codewarrior and when you are installing it you need to select the S08 devices.

I hope this will help you

0 Kudos
Reply
4,085 Views
w_lingjun
Contributor III

Hi Vicente,

Thank you very much!

Sorry for replying so late. I just installed S12Z family when I did some work on MC9S12ZVML128. It is too big to install all family~

Beat regards,

Sarah

 

0 Kudos
Reply