Does CodeWarrior 11 support MC9S08SG8?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does CodeWarrior 11 support MC9S08SG8?

ソリューションへジャンプ
4,094件の閲覧回数
w_lingjun
Contributor III

Hi,

When I new a bare board project in CodeWarrior 11, I can't find this MCU: MC9S08SG8 on devices interface.

So does CodeWarrior 11 support MC9S08SG8?

Best regards,

Sarah

0 件の賞賛
返信
1 解決策
4,078件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I believe that the problem was on the installation, you do not have installed the S08 family, the easier solution is to reinstall Codewarrior and when you are installing it you need to select the S08 devices.

I hope this will help you

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,091件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Yes

 

vicentegomez_0-1607348148178.pngvicentegomez_0-1607348148178.png

You should have it.

 

Regards

Vicente G

0 件の賞賛
返信
4,085件の閲覧回数
w_lingjun
Contributor III

Hi Vicente,

Thanks for your reply.

This is my CW  version page

cw11_version.pngcw11_version.png

And this is the devices select interface when new a project, there is no HCS08SG Familly.

cw11_1.pngcw11_1.png

And I and can't search any devices when input MC9S0.

cw11_0.pngcw11_0.png

Is there any update packages should I install?

 

Best regards,

Sarah

 

0 件の賞賛
返信
4,079件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I believe that the problem was on the installation, you do not have installed the S08 family, the easier solution is to reinstall Codewarrior and when you are installing it you need to select the S08 devices.

I hope this will help you

0 件の賞賛
返信
4,049件の閲覧回数
w_lingjun
Contributor III

Hi Vicente,

Thank you very much!

Sorry for replying so late. I just installed S12Z family when I did some work on MC9S12ZVML128. It is too big to install all family~

Beat regards,

Sarah

 

0 件の賞賛
返信