Device Initialization / PE in CW10.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device Initialization / PE in CW10.3

ソリューションへジャンプ
1,566件の閲覧回数
ralphi
Contributor I

Hi folks!

some time ago I have done a project with the S08GT16A in CW6.3. There I've used the Device Intitialization to setup all needed modules, frequencies and so on. It is a very nice tool also to look up details like ADC conversion time etc. resulting from my clock settings.

 

Some years later now, my colleagues told me that eclipse is the tool to use (they use it with gnu-c for arm)... So I've installed CW10.3 and tried to import my old project... After many trial and error I began reading this forum and found out that CW10.2 seems to be the last version which had an import function for old CW classic projects. Then I've found a CW 10.0 installation file on my HD. So I've installed CW10.0. After "cleaning" a copy of my CW6.3 project (by mistake I deleted also the project.map file), I've started the import process. After some minutes I had a converted project which I saved and then started CW10.3 and loaded my converted project. Some settings weren't correct, but after some modifications in the properties I could work and compile and flash the GT16A. Then I've tried to change some settings for the Ports and the ADC. How can I do that? In CW6.3  it is still very easy and I can CW let generate a new MCUinit.asm. But I think that is not "the" way to do changes or am I wrong? Since I was in a hurry, I've changed the MCUinit.asm by hand then. So now my question, how can I do these tasks with CW10.3 (or 10.4 if it works better)???

 

My last trial was to import the project again (now with the project.map) but up to now I've found no possibility to look at or change my hardware settings. Is this not possible because I am using the Special Edition?

 

I could try to start a new project and copy my source files to it, but then I would have to do all my settings again in PE... If it is possible at all...

 

Every help is appreciated!

 

Best regards,

Ralph

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,407件の閲覧回数
Rick_Li
NXP Employee
NXP Employee


it looks like that you are using assembly as your application language in CodeWarrior v6.3.

if you want to use a Eclipse based CodeWarrior, then, I would suggest using the latest version 10.4.

Since the Device Initialization tool is no longer supported after CW v10.3, it would be better if you could using C as your language.

it would also easy to set ADC in PE, the setting is alomst same with that in Device Initialization.

please let me know if you need further help?

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,408件の閲覧回数
Rick_Li
NXP Employee
NXP Employee


it looks like that you are using assembly as your application language in CodeWarrior v6.3.

if you want to use a Eclipse based CodeWarrior, then, I would suggest using the latest version 10.4.

Since the Device Initialization tool is no longer supported after CW v10.3, it would be better if you could using C as your language.

it would also easy to set ADC in PE, the setting is alomst same with that in Device Initialization.

please let me know if you need further help?

0 件の賞賛
返信