DEMOFLEXISJMSD  schematic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEMOFLEXISJMSD  schematic

ソリューションへジャンプ
3,164件の閲覧回数
PO220
Contributor IV

Hello

 

I'm looking for DEMOFLEXISJMSD and the demo software of this page

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMOFLEXISJMSD&fsrch=1

 

Can you confirm me that the hardware for this part is the same than the hardware described in DRM104 "SD Card Reader Using the M9S08JM60 Series"

 

If not, where can I find the schematics for DEMOFLEXISJMSD. It's not easy to buy it in France... 

 

Thank you in advance.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,043件の閲覧回数
peg
Senior Contributor IV

Hello,

 

There are a couple of links that should go to a pdf of the schematic of this, but the PDF seems to be broken.

 

Right click on the link and download it as a text document. When you have it on your machine change the extension to pdf and now it works!

 

Message Edited by peg on 2009-08-28 07:19 PM

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,044件の閲覧回数
peg
Senior Contributor IV

Hello,

 

There are a couple of links that should go to a pdf of the schematic of this, but the PDF seems to be broken.

 

Right click on the link and download it as a text document. When you have it on your machine change the extension to pdf and now it works!

 

Message Edited by peg on 2009-08-28 07:19 PM
0 件の賞賛
返信
2,043件の閲覧回数
PO220
Contributor IV

Thank you very much

 

 

0 件の賞賛
返信
2,043件の閲覧回数
J2MEJediMaster
Specialist I

Thanks for the workaround, peg. It looks like maybe the MIME type or file extension is messed up on this file. I am reporting it to IT to get this corrected. You folks should not have to resort to minor rocket science to obtain the schematic.

 

---Tom

0 件の賞賛
返信