DEMO9S08SH32 Pointers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEMO9S08SH32 Pointers

ソリューションへジャンプ
2,711件の閲覧回数
Coyote
Contributor I

Hello,
I am new to this forum, I bought a DEMO9S08SH32 to various tests.
 I have a problem with pointers in language C, for example:

int *p1;

(void) main(void)
{

 ----

 *p1= 0;

 ----
}

The result to CodeWarrior is: *p1= 0x2e00 ?
I think normaly is: *p1= 0x0000 !

Thany you for your answer.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,887件の閲覧回数
tonyp
Senior Contributor II

p1 is a(n uninitialized) pointer to an integer, not the variable that actually holds the value.

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,888件の閲覧回数
tonyp
Senior Contributor II

p1 is a(n uninitialized) pointer to an integer, not the variable that actually holds the value.

 

0 件の賞賛
返信
1,887件の閲覧回数
Coyote
Contributor I

Thank you for your answer, if I understand "int *P1" is only a variable that contains the adress of variables!

0 件の賞賛
返信