DEMO9S08QE8UM Demo Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEMO9S08QE8UM Demo Board

1,615 Views
DavidoBG
Contributor II
With DEMO9S08QE8UM kit, is it possible to put MC9S08QE8 with 16 pins package on daughter board?
 
thanks
 
david
Labels (1)
0 Kudos
Reply
1 Reply

976 Views
Ake
Contributor III
Hi,
The daughterboard for the 9S08QE8 is a 32 pin device and P&E has used more than the minimum number of pins to hook up the USB interface to it.
So to be able to use the BKGD pin, you will have to buy either the USB Multilink or the Cyclone Pro to do it.
 
Regards,
Ake
0 Kudos
Reply