Code Warrior code window - JM60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior code window - JM60

3,801件の閲覧回数
donw
Contributor IV

when I use CW to assemble code (assembler code only) using the 'Make' or 'Debug'

buttons, when complete it shows the message 'project all up to date' at the top of

the source code window & hides the source code.

This is a bother, since I then have to click on the .asm file name

to make the source code reappear.

Is there some way to keep the source code visible?

Message Edited by NLFSJ on 2009-08-18 10:01 AM
Added p/n to subject.
Message Edited by NLFSJ on 2009-08-18 10:01 AM
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,260件の閲覧回数
CrasyCat
Specialist III

Hello

 

- Which version of CodeWarrior are you using?
To retrieve that info:
   - Start CodeWarrior
   - Select Help -> About Freescale CodeWarrior
   - Click on "Install Products"
   - CodeWarrior version used is displayed on top in the Installed Products dialog.

CrasyCat

0 件の賞賛
返信

2,260件の閲覧回数
donw
Contributor IV

version is IDE 5.9.0 build 2404

The message appears in a window which overlays the code window, hence you have to click on the source code filename or Ctrl-Tab back to that screen. 

 

0 件の賞賛
返信

2,260件の閲覧回数
CrasyCat
Specialist III

Hello

 

This does not help to identify the product you are using.

As stated in my last message, to retrieve that info:
   - Start CodeWarrior
   - Select Help -> About Freestyle CodeWarrior 
   - Click on "Install Products"
   - CodeWarrior version used is displayed on top in the Installed Products dialog.

 

Did you maximize the source window inside of CodeWarrior?

Is the issue reproducible if you restore source window to its original size?

 

CrasyCat

0 件の賞賛
返信

2,260件の閲覧回数
donw
Contributor IV

CW dev studiov6.1 build 7285 -20 oct 07

JM60 service pack build 071128

 

I have maximised the code window . (And why is it not max'ed on startup!?)

I think this window action is normal, but it is annoying since after a build you have to Cntl-Tab back to the code window. (even though the result window only  takes up the top part of the screen)

 

-If I install a newer version  of CW do I have to reinstall the JM60 service pack?

0 件の賞賛
返信

2,260件の閲覧回数
CrasyCat
Specialist III

Hello

 

Maximizing the code window will maximize all the windows opened in CodeWarrior.

I would recommend you to remove the maximized and just change size of the window and make it bigger.

 

CrasyCat

0 件の賞賛
返信