Can we use multi-link programmer tools to program MM9Z1J638BM2EP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use multi-link programmer tools to program MM9Z1J638BM2EP?

Jump to solution
3,613 Views
chitsanupong_ng
Contributor II

Can we use multi-link programmer tools to program MM9Z1J638BM2EP?

If yes, can you tell me a software tools that support like this, please?

Labels (1)
0 Kudos
Reply
1 Solution
3,358 Views
chitsanupong_ng
Contributor II

Hello,

I do following on previous post as link below. the failure is gone. So for my conclusion of this failure.

we need to add a capacitor 470uF connect between #RESET (pin 2) and GND (Pin 4) for protect the analog die watchdog issue.

"Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P... 

pastedImage_5.png

View solution in original post

0 Kudos
Reply
6 Replies
3,358 Views
vicentegomez
NXP TechSupport
NXP TechSupport

HiYes you can use the Multilink to programm it, and you can use codewarrior 11 as IDE.

Hope this will help you.

Regards

0 Kudos
Reply
3,358 Views
chitsanupong_ng
Contributor II

Ok, I will try and update result soon. Thanks

0 Kudos
Reply
3,358 Views
chitsanupong_ng
Contributor II

Hello,

We found the device can't erase due to device is secure and we click "yes" the software has show figure 2 and then we did follow the message show, the figure 1 is repeating and we re-do again. the result has show on figure 3. how are we gonna fix for this failure?

pastedImage_1.png

Figure 1

pastedImage_2.png

Figure 2

pastedImage_3.png

Figure 3

0 Kudos
Reply
3,358 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Did you perform a power cycle? you need to unplug the device and the multilink that plug again and retry.

I hope this will help you

0 Kudos
Reply
3,358 Views
chitsanupong_ng
Contributor II

Yes, we did either multilink and the device the message still failed as picture below.pastedImage_2.png

0 Kudos
Reply
3,359 Views
chitsanupong_ng
Contributor II

Hello,

I do following on previous post as link below. the failure is gone. So for my conclusion of this failure.

we need to add a capacitor 470uF connect between #RESET (pin 2) and GND (Pin 4) for protect the analog die watchdog issue.

"Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P... 

pastedImage_5.png

0 Kudos
Reply