Can we use multi-link programmer tools to program MM9Z1J638BM2EP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can we use multi-link programmer tools to program MM9Z1J638BM2EP?

跳至解决方案
3,777 次查看
chitsanupong_ng
Contributor II

Can we use multi-link programmer tools to program MM9Z1J638BM2EP?

If yes, can you tell me a software tools that support like this, please?

标签 (1)
0 项奖励
回复
1 解答
3,522 次查看
chitsanupong_ng
Contributor II

Hello,

I do following on previous post as link below. the failure is gone. So for my conclusion of this failure.

we need to add a capacitor 470uF connect between #RESET (pin 2) and GND (Pin 4) for protect the analog die watchdog issue.

"Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P... 

pastedImage_5.png

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,522 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

HiYes you can use the Multilink to programm it, and you can use codewarrior 11 as IDE.

Hope this will help you.

Regards

0 项奖励
回复
3,522 次查看
chitsanupong_ng
Contributor II

Ok, I will try and update result soon. Thanks

0 项奖励
回复
3,522 次查看
chitsanupong_ng
Contributor II

Hello,

We found the device can't erase due to device is secure and we click "yes" the software has show figure 2 and then we did follow the message show, the figure 1 is repeating and we re-do again. the result has show on figure 3. how are we gonna fix for this failure?

pastedImage_1.png

Figure 1

pastedImage_2.png

Figure 2

pastedImage_3.png

Figure 3

0 项奖励
回复
3,522 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Did you perform a power cycle? you need to unplug the device and the multilink that plug again and retry.

I hope this will help you

0 项奖励
回复
3,522 次查看
chitsanupong_ng
Contributor II

Yes, we did either multilink and the device the message still failed as picture below.pastedImage_2.png

0 项奖励
回复
3,523 次查看
chitsanupong_ng
Contributor II

Hello,

I do following on previous post as link below. the failure is gone. So for my conclusion of this failure.

we need to add a capacitor 470uF connect between #RESET (pin 2) and GND (Pin 4) for protect the analog die watchdog issue.

"Device is secure. Erase to unsecure?" error message comes up when I try to program MM9Z1J638 with P... 

pastedImage_5.png

0 项奖励
回复